I have TI P/N: TMDSCCS-MCUN01-v4.0
It is described the as full version of Microcontroller - Node Locked which is identified as (Licensed) at the top of the program when running ( License file on hard drive). This version should support ARM by what I have read.
I talked to my TI rep. about the fact that I can not use this version for ARM products. He stated that I may not have activated the ARM option when I installed the program. I can not run the DVD to upgrade or install the ARM option, nor can I go to Add/Remove to change CCS. Here are the details of what I have:
Help > About CCS > Version: 4.2.3.0004
Here is what is existing for types of uC:
File > New > CCS Project > Name > Next > Project Type: Only MSP430 and C2000 show up, not ARM.
? How do I activate the ARM products in this version without starting over?
Thanks