Hello,
I use AWR1843, XSD110 debugger and ccs software to build a debugging environment, and use python to write scripts to call the methods in the DSS interface to achieve automated testing. When the target board is running, the script execution shows a timeout and throws an exception, but when the CCS software is used for manual operation, the development board can run successfully. The script execution content is the same as the manual operation process. I want to know what causes this error timeout? Please help everyone, thank you!The screenshot of the error report and the content of the script are as follows: