This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO-SITARA: Error occurred when connecting XDS560v2

Guru 15520 points

Part Number: CCSTUDIO-SITARA
Other Parts Discussed in Thread: AM3356

Hi,

My customer is having some issue when connecting the AM3356(customer board) to CCS via XDS560v2 System Trace(Blackhawk).
Their environment is :
CCS v8.1.0.00011 is installed on Ubuntu 18.04.
At target configuration, they are selecting "Blackhawk XDS560v2-USB System Trace".

When they tried to connect, the following error occured:
************************************************
[Start: Blackhawk XDS560v2-USB System Trace Emulator_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]

-----[Print the board config pathname(s)]------------------------------------

/home/user/.ti/ti/0/0/BrdDat/testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'libbh560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: open failed: code 19
Download failed for file /home/mito/ti/ccsv8/ccs_base/common/uscif/./././././xds560v2.out

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.

The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.

[End: Blackhawk XDS560v2-USB System Trace Emulator_0]
**********************************************************************

What is causing such error?
How to solve this issue?

best regards,
g.f.