Part Number: CODECOMPOSER
Other Parts Discussed in Thread: SYSCONFIG
While trying to build a project from my company, my Windows machine is unable to build the project due to the below errors shown in the given screenshot. Although the warnings show that some objects are undefined, that is not the case based on the code. Hence I am not sure where the issue is occurring. Note: For the error for GIT_HASH occurs in comm.c however the macro defined in sensors.c
Compiler: TI v18.1.5.LTS
SDK: SimpleLink CC13x2 26x2 SDK v3.10.0.53
XDCTools v3.50.8.24_core

Errors Transcribed:
gmake: *** [all] Error 2
gmake[1]: *** [comm.obj] Error1
gmake[1]: Target 'main-build' not remote because of errors
#66 expected a ";" Location: Line 211 ~.\CryptoKey.h
#20 identifier "CryptoKey_Encoding" is undefined Location: Line 211 ~.\CryptoKey.h
#20 identifier "CryptoKey_Encoding" is undefined Location: Line 240 ~.\CryptoKey.h
#20 identifier "GIT_HASH" is undefined Location: Line 813