This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Watch points do not work on CCS 5.1 M4



Hi,

 

Here is my setup:

OS: Ubuntu 10.04

CCS: 5.1 M4 5.1.0.04001

Emulator: Spectrum Digital XDS 560v2 STM USB

I've been trying to set watchpoints, but the debugger never stops on them. I tried the same tagret board and the same emulator with CCS 4.1.3 on Windows machine and it works fine.

BR,

--Michael