I don't use Internet Explorer or Outlook/Outlook Express and have set the "use external browser" to firefox. However, CCS still tries to send exception reports using some Microsoft program (I get a warning with the ie logo) which of course doesn't work as there is no e-mail defined there. CCS also still opens Internet Explorer so I have to copy the link over to Firefox and open it there (Internet Explorer is ONLY allowed to talk to Microsoft Update).
Is there a way to fix this or is this just because someone used Microsoft tools to create CCS?
System:
Windows XP
Firefox 4.0.1 (set as default browser)
Thunderbird 3.1.10 (set as default mail)