My platform is C6A816X/AM389X DDR2,when I want to connect to DSP of board, I found that TI 816X device have not C674X device, instead it, the DSP family is 64XP, refer to the picture. I want to connect the DSP device,what should I do?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My platform is C6A816X/AM389X DDR2,when I want to connect to DSP of board, I found that TI 816X device have not C674X device, instead it, the DSP family is 64XP, refer to the picture. I want to connect the DSP device,what should I do?
Thanks!
Hi Ralph,
When I update to CCS5.03, the DSP target change from C64X to C674X, But I can not connect the DSP device also. The error as follows:
Error connecting to the target:
The target is being held in reset. The applied reset must be released before progressing.
(Error -1180) @ 0 (0x0)
Error connecting to the target:
Invalid data was scanned by the emulation controller.Verify the board setup to make sure the scan chain is properly defined. If the setup is correct, then RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target.
(Error -1146) @ 0 (0x0)
I what to know what Emulator do you use? My emulator is XDS560, and what should I do?
Thanks!
Anyone can help me! If someone have the same problem, please contact me!
Thanks!
Anyone can help me! If someone have the same problem, please contact me! Thanks!
Hi ,
I encountered a simiplar problem and can you tell me where to set the speed ?
I set mine to adaptive with a limit of 10. I could probably go higher but I am running mine over the LAN and this seems to work well. Settings are below: