Is there support for the Klocwork plug-in in CCS4? I have installed the plug-in which added a "Klocwork" and "Klocwork Build Settings" option to my project properties. But when I select either option, I get a 'Property Page Creation Problems" dialog with this verbiage: Unable to create the selected property page. Reason: Plug-in com.klocwork.eclipsedeveloperenterprise was unable to load class com.klocwork.inforceeclipseide.preferences.ProjectBuilSettingsPage. Any help in getting the plug in to work? Thanks!!