Other Parts Discussed in Thread: CCSTUDIO
Hello,
How to get c54x environment simulated. I tried in both CCS 3.3 and CCS4 . I could not get it. Please help me with that.
Thanks
Suresh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CCSTUDIO
Hello,
How to get c54x environment simulated. I tried in both CCS 3.3 and CCS4 . I could not get it. Please help me with that.
Thanks
Suresh
Suresh,
Unfortunately both CCSv3.3. and 4 do not support C54x simulators. Please check the page below:
http://processors.wiki.ti.com/index.php/List_of_Simulator
Regards,
Rafael
Thanks Rafael. So Is there any older version of CCS which supports C54x simulation? My concern to use C54x simulator is to understand the functionality of C54x intrinsics and port it to C64x. Is there any way to simulate them?
Thanks in advance
Suresh,
Sorry about my previous reply - I was misled by a rather incomplete wiki page (I am fixing it).
Yes, CCSv3.3 supports several C54x device simulators and you can use it to verify the functionality of the compiler intrinsics.
Regards,
Rafael
Rafael,
Thanks. When I create a project I am able to select c54x simulator. Ansd also I am able to build a basic program without errors. But when I try to run , I am getting an error "Warning ! No Valid program is currently loaded into memory.Do you still want to run ?" . If I click yes, it is pointing to some garbage location. If I click NO, it is exiting.
Am I missing , something.
Thanks
Suresh
Rafael, Thanks. When I create a project I am able to select c54x simulator.
Ansd also I am able to build a basic program without errors. But when I
try to run , I am getting an error "Warning ! No Valid program is
currently loaded into memory.Do you still want to run ?" . If I click
yes, it is pointing to some garbage location. If I click NO, it is
exiting. Am I missing , something. Also I could not create .cmd file. The reason is when I try to create a BIOS configuration file, I couldnt see an option to select C54x simulator platform. Is this the reason I couldnot run my code? Thanks Suresh
Rafael, Thanks. Also, I tried using the example project provided by TI located at my local disk : " CCStudio_v3.3\C5400\dsplib\EXAMPLES\ADD" . Even with this I am getting the same error "Warning ! No Valid program is
currently loaded into memory.Do you still want to run ?" . If I click
yes, it is pointing to some garbage location. If I click NO, it is
exiting. Thanks Suresh
Suresh,
After building your project you need to load it to the simulator (as if you were loading your code to a board via an emulator). Go to menu File --> Load Program and point to the .out file generated.
Hope this helps,
Rafael
P.S. The list of simulators page is fixed now.