I have my target configuration set to not connect automatically when it's launched. When I launch a target configuration (in this case for TI 8148EVM) all seems to go well. After it launches I wait few moments, then I right click on the target processor in the Debug window and select "Connect Target". At this point CCM (eclipse) just disappears. When I look into the process table the eclipse process is gone. I'm not sure what info might be useful for you folks. The "Troubleshooting CCS" wiki page doesn't seem to have anything specific for CCS v5.1, so I attached the config file and the log file which I got from the about menu.