To anyone:
I installed CCSV5.0 recently and have many problems with it .
I created a project and use the IPC multicore notify module template which had been created the same way in CCSV4.2 ,I run successfully in ccsv4.2,but in ccsv5.0 i has got a lot of problems, i tried to solve some ,but still can not successfully build the project ; Now my problem is "cannot open command file '/configpkg/compiler.opt' ";
I had view the ccs4 to v5 changes,but still do not known why this happened;
Also, each time I run a program, it appear a window and says cannot find file (e.g. 'exit.c' or 'Idle.c' or 'Hwi_stack.c') , I locate the file address and it run into those files; Is it necessary to do so ? will this affect the result of program? Am i need to do so each time it appears?
thank you for reply