Other Parts Discussed in Thread: MSP430FR5994
Dear all,
I'm using CCS version 11.2 to develop code for the MSP430FR5994. I'm using different build targets which are calling a self-made build script. Under project properties/Build/Builder I modified the Build command to be "bash ${ProjDirPath}/scripts/build.sh", where the build.sh is a self-made script which is also used by the a build server for automatic building and continuous integration. This script supports different commands, like "build.sh clean", "build.sh cmake", "build.sh application" and several others, where each command executes a specific task only. So the clean command obviously cleans the project output folder by just deleting everything. The cmake command generates all the makefiles using CMake and a CmakeLists.txt. The application command then builds the application using the generated makefiles. So far so good.
Then I created some "Build Targets" within CCS. They appear in the project explorer and can be used to build different targets, namely to run the script with the specific commands like cmake or application. But when I run one of those build targets CCS automatically runs the clean command first for each build target and I don't know why. So when I run the application build target, everything gets deleted just before including the generated makefiles that I created previously using the cmake command end the application can't be built. The console output would look like this:
**** Clean-only build of configuration Debug for project Prj ****
bash D:/Projects/Prj /SW/Prj/scripts/build.sh clean
Script path: /cygdrive/d/Projects/Prj/SW/Prj/scripts
==== Project path: /cygdrive/d/Projects/Prj/SW/Prj
==== Building Project - Server; Wed Sep 28 13:16:17 WEDT 2022 =======================================
==== Cleaning up and delete /cygdrive/d/Projects/Prj/SW/Prj/build/Debug/test
==== Cleaning up and delete /cygdrive/d/Projects/Prj/SW/Prj/build/Debug/main/DevKit
==== Cleaning up /cygdrive/d/Projects/Prj/SW/Prj/reports
**** Build Finished ****
**** Build of configuration Debug for project Prj ****
bash D:/Projects/Prj/SW/Prj/scripts/build.sh application
I want CCS to only call the second command line "bash D:/Projects/Prj /SW/Prj/scripts/build.sh application", but it automatically runs the first line "bash D:/Projects/Prj /SW//Prj/scripts/build.sh clean" as well and everything gets erased just before the build starts. Then there is an error because there are no makefiles. Is there a way to disable this? Why does CCS do that?
Thanks and best regards,
Marco