Hi,
I currently use a C55BootImage.exe GUI program to convert .OUT files to .BIN files for flashing application code to flash memory.
Is there a way to integrate this program (which also accepts command-line parameters), seemlessly into CCS12, a bit like the HEX utility is proposed as shown below ??

Would it be possible to replace the "command" entry above, with the C55BootImage.exe program (or change the path variable) and provide it the required in/out parameters etc ?? Just wondering if this might work ??
Thanks, Mike