This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unknown CCS error



I have come across an error while working with the LAUNCHXL-CC26XR1 trying to flash an alteration of project 0 to the MCU. I first get an error shown below when trying to flash. If I press retry, CCS crashes before the flash is complete. If I hit cancel, then CCS crashes that next time I try to flash the device. I am using CCS 12.1 and have tried versions 6.30.00.84 and 6.30.01.03 for importing the project 0 example. Is there any known issue for this error or any known solutions?

Error initializing emulator:
(Error -261 @ 0x0)
Invalid response was received from the XDS110.
(Emulation package 9.9.0.00040)