This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am currently using Code Composer Studio Core Edition (vers. 4.2.3.00004) on Windows XP to program an evaluation board with MSP430 through MSP-FET430UIF. After I upload the program in the target board I am not able to run the debugger; the option Target -> Run is disabled. All the options related to the debugger (Halt, Step into, etc.) are disabled). Even the Target -> Connect Target is disabled. Should I reinstall the USB-Debug interface (MSP-FET430UIF)?
Thank you.
Regards,
Gaspare
Hello Gaspare,
This can happen if you close the Debug view. See the below FAQ:
Thanks
ki
Hello Ki,
Thank you for your reply.
Yes, the problem was related to the debug view.
Thank you.
Regards,
Gaspare