This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS compilation in command line issue using a Docker

Hi,

Trying to compile a CCS project in a Docker. Compiling it in command line on a pc works ok ( using this doc : https://software-dl.ti.com/ccs/esd/documents/ccs_projects-command-line.html#working-with-ccs-linux )

 But while trying it in a Docket  the following error appears :

---------------------------

Unable to init server: Could not connect: Connection refused

Eclipse:

An error has occurred.

---------------------------

Below the log messages :

----------------------------------------------------

eclipse.buildId=4.14.0.I20191210-0610

java.version=1.8.0_112

java.vendor=Oracle Corporation

BootLoader constants: OS=linux, ARCH=x86_64, WS=gtk, NL=en_US

Command-line arguments:  -os linux -ws gtk -arch x86_64

 

!ENTRY org.eclipse.osgi 4 0 2023-01-30 15:32:07.388

!MESSAGE Application error

!STACK 1

org.eclipse.swt.SWTError: No more handles [gtk_init_check() failed]

        at org.eclipse.swt.SWT.error(SWT.java:4746)

        at org.eclipse.swt.widgets.Display.createDisplay(Display.java:1117)

        at org.eclipse.swt.widgets.Display.create(Display.java:1057)

        at org.eclipse.swt.graphics.Device.<init>(Device.java:175)

        at org.eclipse.swt.widgets.Display.<init>(Display.java:623)

        at org.eclipse.swt.widgets.Display.<init>(Display.java:614)

        at org.eclipse.ui.internal.Workbench.createDisplay(Workbench.java:778)

        at org.eclipse.ui.PlatformUI.createDisplay(PlatformUI.java:166)

        at org.eclipse.ui.internal.ide.application.IDEApplication.createDisplay(IDEApplication.java:180)

        at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:123)

        at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)

        at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:137)

        at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:107)

        at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401)

        at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)

        at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)

        at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)

        at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)

        at java.lang.reflect.Method.invoke(Method.java:498)

        at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:657)

        at org.eclipse.equinox.launcher.Main.basicRun(Main.java:594)

        at org.eclipse.equinox.launcher.Main.run(Main.java:1465)

        at org.eclipse.equinox.launcher.Main.main(Main.java:1438)

--------------------------

The problem appears because there is no X11 server in the Docker. When the command on the PC is run no GUI display appears so could not understand why it tries to createDisplay.

 Is there an option to avoid using graphical commands ?

Thank you!

Best regards,

Guillaume