Hi all,
In CCS, optimization can be set globally for all files by right clicking on a project->Properties->CCS Build->Arm Compiler->Optimization (correct for the MSP432 we use, I guess it might be different for different controllers).
This project wide setting can be overriden for any given file in the project by right clicking on the file and settings its optimization as described above.
In a large project, it can be hard to keep track of which files have overrides (for optimization or other build settings).
I see that files that have ever had overrides get a little key in their icon, but if you create an override, then remove it, the key icon seems to stay permanently, so this doesn't necessarily help.
Is there a way of generating a summary indicating which files have build settings that are different to the global build settings (and list out what those differences are)? The only way I can find to do this currently is to manually look at the properties of each file - time consuming with nearly 100 files in the project....
Thank you!
Julian