This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS run same makefile multiple times

Part Number: CCS
Other Parts Discussed in Thread: CC1312R

If i start a project build in CCS some dependent projects are build multiple times:

**** Build of configuration Debug-6.10 for project libConfig ****
**** Build of configuration Debug-6.10 for project libIZW ****
**** Build of configuration Debug-6.10 for project libLogger ****
**** Build of configuration Debug-6.10 for project libLogger ****
**** Build of configuration Debug-6.10 for project libLogRf ****
**** Build of configuration Debug-6.10 for project libRF ****
**** Build of configuration Debug-6.10 for project tirtos_cc1312r1 ****
**** Build of configuration Debug-6.10 for project libConfig ****
**** Build of configuration Debug-6.10 for project libIZW ****
**** Build of configuration Debug-6.10 for project libLogger ****
**** Build of configuration Debug-6.10 for project libLogRf ****
**** Build of configuration Debug-6.10 for project libRF ****
**** Build of configuration Debug-6.10 for project tirtos_cc1312r1 ****

**** Build of configuration Debug-6.10 for project loggerRFstream ****

Every referenced modul is build 2 times, and libLogger is build 3 times.

The defined dependencies are:

  • loggerRFstream: libIZW, libLogger, libRF, libConfig, tirtos_cc1312r1, libLogRf
  • libIZW: -
  • libLogger: -
  • libRF: -
  • libConfig: -
  • tirtos_cc1312r: -
  • libLogRf: libLogger

Has anyone any idea what's going wrong? Or any idea how to debug the build order?

  • Hello,

    Is this something that was working and then started to have issues? Or was this always an issue?

    Can you also share just the main project's .metadata (the three .*project files in the project folder)?

    Thanks

    ki