Other Parts Discussed in Thread: OMAP-L138, TMS470MF03107, TMS470MF04207, TMS470MF06607
Hi,
Under CCS4, what compiler should be selected to compile OMAP-L138 Arm code?
KB2603
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L138, TMS470MF03107, TMS470MF04207, TMS470MF06607
Hi,
Under CCS4, what compiler should be selected to compile OMAP-L138 Arm code?
KB2603
TMS470.. covers all ARM variants TI supplies.
Regards
Thx for your response.
From the Build menu of a project, I can see a list of device starting with "TMS470":
TMS470MF03106
TMS470MF03107
TMS470MF04207
TMS470MF06607
TMS470MF06608
TMS470MSF542
Which one corresponds to OMAP-L138 ARM?
Thx
KB
None. You need to select " Generic ARM9 Device" in the build properties. See the CCS Build/General tab -> Device Variant.
Make sure that C/C++ Build/TMS470 Compiler/Basic Options has the target processor version set to '5e'.
That should take care about your ARM side compiler to generate ARM9 code.
Frank,
Thx for your response.
I wanted to make sure I was using the right compiler for the OMAP L138 ARM926ejs core.
I see sometimes in source code (mainly in the boot.asm code of LED blink example) some constants such as:
__TI_TMS470_V7M3__
__TI_EABI_ASSEMBLER
__TI_ARM9ABI_ASSEMBLER
.TMS470_32BIS
.TMS470_16BIS
__TI_NEON_SUPPORT__
__TI_VFP_SUPPORT__
Do you know where those constants are defined?
I checked the version of ARM9 compiler installed: TI v4.6.3
Rgds
KB
To my knowledge the constants are defined by the compiler depending on code generation and optimization settings.
Regards.