This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

_itof issue in TI C6000 compiler 8.3.12



Problematic code:

float lower16BitAsFloat_incorrect(uint32_t a)
{      
    const uint32_t lo16 = a & 0x0000FFFFU;
    return _itof(lo16);
}

float lower16BitAsFloat_correct(uint32_t a)
{      
    return _itof(a & 0x0000FFFFU);
}

We expect both functions to producce functionally identical target code.

Calling the compiler with the following flags: -mv6600 --c++14 -O3 -DNDEBUG --auto_inline=0 -ms1
produces wrong output for the first function. Note the missing EXTU instruction in lower16BitAsFloat_incorrect:

lower16BitAsFloat_incorrect(unsigned int):
           RETNOP          B3,5              ; [] |14|

lower16BitAsFloat_correct(unsigned int):
           RETNOP          B3,4              ; [] |26|
           EXTU    .S1     A4,16,16,A4       ; [A_S66] |25|

Trying to narrow down the triggering condition, we found that the following code produces correct binaries.

So, we suspect, that the issue is related / limited to 16-bit handling and is not triggered because of a FP subnormal pattern.

float lower17BitAsFloat_correct(uint32_t a)
{      
    const uint32_t lo17 = a & 0x0001FFFFU;
    return _itof(lo17);
}

float lower15BitAsFloat_correct(uint32_t a)
{      
    const uint32_t lo15 = a & 0x00007FFFU;
    return _itof(lo15);
}

Produces:

lower17BitAsFloat_correct(unsigned int):
           RETNOP          B3,4              ; [] |8|
           EXTU    .S1     A4,15,15,A4       ; [A_S66] |7|

lower15BitAsFloat_correct(unsigned int):
           RETNOP          B3,4              ; [] |20|
           EXTU    .S1     A4,17,17,A4       ; [A_S66] |19|