Hi all!
I am a newcomer to CCS family and was so excited about working with the MSP430 FRAM family. Unfortunately, I ran right into an issue which I have not been able to resolve on my own by searching in the various FAQs and forum discussions. Might have been, because I oversaw the most obvious points, which I apologize for in advance.
The issue can be described as follows:
I purchased a MSP-EXPFR5379 kit and downloaded CCS 4.2.3. Installation of the tool on Windows XP SP2 and registration went well, I got a license file and was able to activate it. Now I can load the demo project MSP-EXP430FR5379 into CCS, make modificartions and recompile, all works fine without issues.
The board is listed under control panel... as "MSP430 Application UART". So the driver seems to be installed correctly.
When I start a debug session and the board is connected, I get a message telling me "You are not licensed to use the currently configured connection-type". When I choose the license file again, then I get an error message telling me that "Excepton occured during launch". Feature "CCS_CONNECTION_ALL" is missing.
Well, the ferature is also not listed in the license file. The file named "TMDSCCS-HWN01A-v4.0.lic" contains a section named "CCS_CONNECTION_RESTRICTED".
How can I resolve the issue and get CCS to work also in debug mode?
Thanks in advance for the support,
Houman