This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with real-time debug mode.

Hi all,

I'm working with F28335 and XDS100 V2 emulator and my project is a 8 kVA AC motor drive.

My problem is when I used "real-time debug mode" to monitor the variable, I got the error:

C28xx: Error: (Error -154 @ 0x0) This utility failed to use the adapter for a custom emulator to perform a write to a controller register. The adapter returned an error. (Release 5.0.333.0)
C28xx: Trouble Halting Target CPU: (Error -150 @ 0x0) This utility failed to operate the adapter for a custom emulator. The adapter returned an error for unknown reasons. (Release 5.0.333.0)

It happens when I turn on the Power circuit.

Plz help me solve this problem.

Thanks and regards,

Hiang Cuong.