Hello,
I am currently running
CCS 9.1.0.00010.
Segger J-link support 7.70.0.0 (ultra+)
I am working with the TIVA TM4C line of ARM M4 microcontrollers.
I have been working with Segger support regarding an emulator issue that occurs. The j-link log files are capturing a RAM check failure. According to Segger 7.70 is out of date and I should be running 7.84, which has improvements regarding this error. A manual software check from the help menu of CCS returns the segger dll is up to date.
Is there a way to force a dll update to the latest 7.86? I found some historical posts from years past in which doing so caused other errors. Can anyone give me a sense of the rabbit hole I am about to embark down?
Thanks in advance!