Other Parts Discussed in Thread: MSP430F1232, MSP430F1611
Using CCSv4, two processors were routinely used in development including debugging: MSP430F1232 and MSP430F1611. After updating CCS (to 4.1.3.00038 and then later to 4.2.3.00004) debugging the MSP430F1232 was normal; but debugging the MSP430F1611 resulted in a “Error connecting to the Target: Could not find device (or device not supported)” error dialog box.
The MSP-FET430UIF pod is used (with 7/8 wire interface to target board; a Softbaugh B1611 development board). It may be important that after both updates, when beginning the first debugging session, the CCS indicated that a FET software update was necessary and this was performed (requiring about 10 seconds).
Manually invoking the debugger worked correctly until connecting to the FET, then the same6558.Connect Problem July2011.doc error message was issued. The USB1 option was selected, and all others gave an error that “…, only found 1 USB FETs”.
Attached are relevant screen print images.