I get the following message when trying to load code into Netra M3 via the Blackhawk USB560
CortexM3_RTOS_0: Warning: (Error -1268 @ 0x1090001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Release 5.0.333.0)
I have previously been able to load and run this code, although always took a few attempts. I have tried power cycling, closing and re-opening tool, resetting CPU etc etc. Configuration file is same as before. Also tried swapping for a different EVM and no different. Another person in my team had this problem and overcame by using a different version of CGTools. I am using version 4.5.1.