Other Parts Discussed in Thread: SYSCONFIG
Don't have a clue where to look to find where this error message is located so I can correct the problem.
subdir_rules.mk:14: recipe for target 'build-807894081' failed Invalid argument '--product': No product with name "MCU_PLUS_SDK_AM62x" and version "08.06.00" found gmake: *** [build-807894081] Error 1 gmake: Target 'all' not remade because of errors.
**** Build of configuration Debug for project test1 ****
/home/fred/ti/ccs1220/ccs/utils/bin/gmake -k -j 16 all -O
Building file: "../untitled.syscfg"
Invoking: SysConfig
"/home/fred/ti/ccs1220/ccs/utils/sysconfig_1.15.0/sysconfig_cli.sh" --script "/home/fred/workspace_v12/test1/untitled.syscfg" -o "syscfg" --compiler ccs
Usage:
cli [-o <dir>] [-s <file>] [-u <string>] [-b <name>] [-d <name>] [-p <name>] [-r <name>] [--treatWarningsAsErrors] [--quiet -q] <script>
cli --help
cli --version
example: cli -s meta_data/sdk.json -d MSP432P401R scripts/two_uarts.js
example: -s sdk.json -d MSP432P401R -o ./display_cfg sdk/cfgs/display.syscfg
Note that the all arguments other than '--help' and '--version' may also be
specified via the script with an embedded @cliArgs comment directive.
E.g. // @cliArgs -d MSP432P401R
If an argument is embedded in a script and explicitly specified via the CLI
then precedence is given to the CLI arguments. Additionally, specifying
"--board" or "--device" on the CLI will override any "--board" and "--device"
arguments specified in the script.
subdir_rules.mk:14: recipe for target 'build-807894081' failed
Invalid argument '--product': No product with name "MCU_PLUS_SDK_AM62x" and version "08.06.00" found
gmake: *** [build-807894081] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****