Other Parts Discussed in Thread: OMAP3530
Hi guys!!
I am working with a OMAP3530, specifically with ARMCortex and an operating system linux running in the device. When the program is builded and linked in CCSv5 , i have doubts about the comunication between operating system Linux and the CCS in order to make the debugging. I have been reading the documentation in this link http://processors.wiki.ti.com/index.php/Linux_Aware_Debug but i have some questions about it: first all, in the options of debugging, do i have to load only the debugging symbols or the program? Then, does the operating system Linux have to run in the beagle board or not yet? Also, the link above discuss about the use of gel files, in principle it is not use but when after i will work with ARM+DSP, so that, will i need this file for this process in the future?
I am very interested in the first two questions so that if anybody can give me any suggestion, it would be great!!!
Thanks in advance!!
Óscar