Other Parts Discussed in Thread: OMAP-L138
Hi,
I've got the following setup/problem with versions CCS_5.1.0.03001 respectivly CCS5.1.0.05000:
- I have two Projects open in CCSv5 (a library project and a "normal" Project)
- the "normal" Project includes the output of the lib-project as library
- the lib-project includes a external folder as linked resource
- the "nomal" Project also includes this linked resource but excludes all sourcen from build (this is just for single-stepping in the parts of the lib)
I can set breakpoints (double-klick) in the sources of the "Linked Folder" but in the editor they are not displayed. When I go to "View -> Breakpoints" I can see the breakpoints beeing set/active. When I try to disable the set and invisible breakpoints, they will be added as another "invisible" breakpoint. See the following screen-shot for more clarity.
Is there a sollution on this problem already available?
regards,
Stefan