This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Log file for Problems window CCS4

CCS 4.2.3

XDC 3.22.1.21

CGTools 6.0.1

DSP BIOS 5.40.10.36

----------------------------------------------------------------------------------------

Hi

I want to generate a log file for all warnings. We only can see 100 warnings together... I try Misra and I have 18600 warnings :P

Is it possible?

Thanks

Jeremy

  • Hi Jeremy,

    This is not supported in v4 but will be supported with CCSv5.1.

    Note that woth v4, you can increase the buffer size of the output console to see more messages. Right-click in the build console view and select 'Preferences' in the context menu. In the dialog that opens, you can increase the max number of lines to display in the console in one of the fields.

    Thanks

    ki