Other Parts Discussed in Thread: SYSBIOS
Hi guys!!
I am working with ARM+DPS architecture and i have doubts about the configuration in order to build programs in DSP with CCSv5.
- First all, i know that is the ARM who to release the DSP from reset throught a function script but the prodecure is complex...I do not know if when i start to create a new project, this project is for ARM or DSP cause both go to perform operations.
- In this connection, I don't know if i have to use gel files for both or only for DSP; I have read in this forum that if I use RTOS for DSP i don't need gel file for DSP..
- I have understood that when you load a program for DSP, CCSv5 loads the program and the real time operating system but the correct procedure I do not now.
- Lasty, can i keep on using gdb server in order to debug for ARM and to use other mode for DSP simultaneously? The goal is to work with ARM and DSP in the same interface, specifically CCSv5
Thanks in advance guys!!
Óscar