This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to link Linear assembly to C++ in CCS3.3 ?

Details on how it has been implemented,but its not working...

1. Judge8- is the linear assembly file.

2. Function prototyping at the begining of the file of a C++-file , where it is called.

Code - as called in C++ file

int Judge8(char idmean, unsigned char *pRGB, unsigned char *imean );

void main()

{

result = Judge8(indexmean, pRGB, imean);

}

 

linear Assembly- Judge8.sa - code is given as below :

.global _Judge8

_Judge8: .cproc indexmean, pRGB, imean

.reg RGB, mean, result1,unpk1, unpk2, dot1,dot2,result,mask

ZERO dot1

ZERO dot2

             ------------------

---------------

 

* On compiling the code it gives a "Undefined symbol for Judge8". Can anybody help if the C++ and linear assembly code have to be linked in any different way on CCS3.3 ??