I have a project that builds fine in Debug mode, but when I switch to Release it is dropping all the -i include directories from the call to the compiler. What is even stranger is if I open one of the files it is compiling and hit Ctrl-F7 to build only that file it compiles fine and the -i include options are all shown. Any ideas? CCS V3.3