This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS and System Analyzer GUI don't work

Hi everyone,

I have a weird problem with the CCS GUI. If I click on 'Tools -> RTOS Analyzer -> Execution Analysis' or 'System Analyzer -> Duration Analysis', nothing happens. No error, just nothing. I used to be able to get to it through the System Analyzer popup by just selecting the execution graph instead. But at some point this also stopped working. I just found out, I can get it to run through 'System Analyzer -> Statistical analysis' and then select the graph there. Update: As I'm typing (and testing this) this also stopped working... So now none of those tools work. The ROV still works. 

I already tried reinstalling the whole CCS (v11.1.xx) but that didn't help.

I can still open the 'Analysis Dashboard' but it shows nothing and if I click on the dropdown in the top down and select 'Execution or Load Analysis', again nothing happens. 

Any ideas? It's a very cool feature which I would very much like to use :D

Greetings,

Max