This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I need a licence



.I am fresh in using the ccs_v5 software. I have downloaded the setup.zip files before.And now I have setted it up on my computer.Without evaluating boards and the software licence,I learn slowly. And 30 days are not enough for me.  I need the software licence and some example codes.

  • there is a possibility to extend the Code Composer Studio licence for another 90 days after 30 days evaluation period expires. I did it for CCSv4. I am sure that same policy is applied for CCSv5. In Help menu of CCS environment, there is "Licence option" and after 30 days just register your installation and prolong your licence for another 90 days. As I mentioned previously, It works for CCSv4. Check it out in your CCSv5 licence option. 

    Regarding to examples, I should choose paltform which you want to use (processor or evaluation board) and many producers of eval boards provide examples of source codes. For example Spectrum Digital company. I use OMAP L137 EVM board, and examples from website can run in simulator as well.

    I hope that it can help  you.

    Roman

  • To expand on Roman's answer, you can also generate a free bundled license. Sounds like you are using simulators since you mention you have no hardware. You can use the free bundled license with simulators. They have no time limit.

    Thanks

    ki