I just installed 5.1 M6 on a CentOS 5.6 machine using the ccs_setup_5.1.0.06000.bin interactive installer. All I need to do is C2000 debugging, so I selected a very minimal install, just C2000 support with XDS100 and Spectrum Digital emulators, but no code generation tools. When I start ccs, a "Problem Occurred" window pops up, with the following details:
An internal error occurred during: "Loading device information".
/opt/TI/ccsv5/ccs_base/common/bin/libfsutiljni.so: /usr/lib/libstdc++.so.6: version `GLIBCXX_3.4.9' not found (required by /opt/TI/ccsv5/ccs_base/common/bin/libfsutil.so)
Do you have a solution or workaround for this problem?
Here are the details for my machine. This is a 32-bit install. Note that I previously was running 5.0.0.00095 on the same machine with limited problems(debugger only). My emulator is a Spectrum Digital XDS510LC.
galens@toto:~$ cat /etc/redhat-release
CentOS release 5.6 (Final)
galens@toto:~$ cat /proc/version
Linux version 2.6.18-238.12.1.el5 (mockbuild@builder10.centos.org) (gcc version 4.1.2 20080704 (Red Hat 4.1.2-50)) #1 SMP Tue May 31 13:23:01 EDT 2011
galens@toto:~$ rpm -q libstdc++
libstdc++-4.1.2-50.el5
thanks,
galen