This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv5: Install / Uninstall / Help - for various components

All

Here is my setup:

- CCS_5.0.3.00028 on Ubuntu 11.04 (VM, if that is of any relevance)

Soon after installing, I ran a few hello-world type apps to convince myself everything was right...

I downloaded and installed (outside of CCS update/install) "bios_6_32_02_39", "ipc_1_23_02_27", "xdctools_3_22_01_21"; I also uninstalled whatever BIOS5, BIOS6 and XDC that came with the original install - by running the uninstall scripts from the respective directories...

# 1. Why is it that I still see old software in the installed list? - RTSC/XDCTools 3.20.6.81 and SYS/BIOS 6.31.4.27

 

 

#2. Is the CDOC (help for installed components) not integrated into Eclipse Help (broken for both Win and Linux versions)?

 

#3. It looks like BIOS6 integration is broken: ex: "File -> New -> DSP/BIOS v5.x configuration file" is available

But, on CCSv4 "File->New->RTSC Configuration File" allows you use BIOS6.

Or, is there another way to create BIOS6 projects?

 

Thanks