I got a question from the customer, regarding ISO26262 certification.
They have the requirement also to certify tool regarding ISO and they have the following questions :
If a Testcase is downloaded from CCS into the RAM of the micro controller, is then the data transfer via JTAG secured by CRC ?
What other mechanisms are used to make sure, that the data transfer carries valid data ?
The same question regarding a register read scenario.
Is the data read out from a register and transferred via JTAG to the CCS on the PC secured by CRC?
Thanks Ralf