Hi
I have installed the ezSDK and Code Sourcery toolchain there after I installed CCS 5.0.3 in Ubuntu 10.04 LTS, Run CCS5 and created a project, but the Project properties does not have a tool chain editor and i can't find how to select the "ARM Linux GCC (Sourcry G++ lite) " tool chain. There are no options either when creating the project.
Where do I get the plugin to intall this so I can select the tool ? I want to start development befor we get the boards from TI. I see it in the sprt601.pdf media pamphlet
Thanks
Robin