This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Warning #10229-D output section ".data" refers to load symbol ".init_array" and hence cannot be compressed; compression "lzss" is ignored.

Part Number: MSP430FR2433

Hi,

I am getting a warning when compiling a simple project. The project compiles ok and works on real hardware but this warning has only just appeared and wasn't there at the start of the project.

Warning #10229-D  output section ".data" refers to load symbol ".init_array" and hence cannot be compressed; compression "lzss" is ignored.

I have 3 structs to control peripherals, which are declared as so:

struct declarations

The memory allocation shows like this:

project memory allocation

My question is: Why does the first struct to be declared, SENSE_L, get put in the .data section and the rest are put in .bss ?

If I swap the SENSE_L and SENSE_R declarations then SENSE_R is placed in .data instead, so it's always the first to be declared that is placed in .data.

This has only just started happening, in earlier versions all were placed in .bss.

The only recent change I have made is to use class enums instead of straight enums and added an operator& override.