Hi ,
I am using 2 BH-USB-2000 with 2- ezdsp28335 boards, and CCStudio 4. I want to know if I can debug 2 projects at the same time using 2 different CCStudio 4 workspace.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
I am using 2 BH-USB-2000 with 2- ezdsp28335 boards, and CCStudio 4. I want to know if I can debug 2 projects at the same time using 2 different CCStudio 4 workspace.
Hi,
I have done this before but with different emulators - i.e., run two CCSv4 sessions with different workspaces debugging different boards/emulators. Thus it is possible from a CCS perspective.
However, from an emulator perspective I am not sure if this model of emulator is able to run two separate instances simultaneously. Did you try to contact BlackHawk?
Regards,
Rafael
hi
thanks Rafael for your reply. I was thinking of contacting BlackHawk but before I do that I want to make sure that its not CCstudio 4 issue.
Hi
I contact BlackHawk and they gave me instructions on how to create 2 different targets configuration and how to connect each of them to a different USB2000 controllers. In this way you will have two target configuration which you can choose to connect to two different projects and debug at the same time.