Other Parts Discussed in Thread: DM3730
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DM3730
#define PACK_STRUCT_BEGIN __attribute__ ((packed))
#define PACK_STRUCT_STRUCT
#define PACK_STRUCT_END
#define PACK_STRUCT_FIELD(x) __attribute__ ((packed, aligned (1))) x
resulting in the following snippet of build message(s):
"S:/Projects/JTSI - Phase 1-2 Technology Dev/Software/CodeWarrior/QP/lwip-1.3.1/src/include/ipv4/lwip/ip_addr.h", line 48: warning: invalid attribute for field "addr" "S:/Projects/JTSI - Phase 1-2 Technology Dev/Software/CodeWarrior/QP/lwip-1.3.1/src/include/ipv4/lwip/ip_addr.h", line 48: warning: a reduction in alignment without the "packed" attribute is ignored "S:/Projects/JTSI - Phase 1-2 Technology Dev/Software/CodeWarrior/QP/lwip-1.3.1/src/include/ipv4/lwip/ip_addr.h", line 64: warning: invalid attribute for field "addrw" "S:/Projects/JTSI - Phase 1-2 Technology Dev/Software/CodeWarrior/QP/lwip-1.3.1/src/include/ipv4/lwip/ip_addr.h", line 64: warning: a reduction in alignment without the "packed" attribute is ignored for the following ip_addr.h file code snippet: PACK_STRUCT_BEGIN struct ip_addr { PACK_STRUCT_FIELD(u32_t addr); //This is line 48 referenced in the warning messages above. } PACK_STRUCT_STRUCT; PACK_STRUCT_END The compiler/linker succeeds in building the application seeming to accept the "packed" attribute for the "PACK_STRUCT_BEGIN" directive on the "struct" definition but when I run the application the LwIP software still generates an ARP packet with extra zero bytes between the MAC addresses in the packet ("packed" attribute has no effect). Interesting how the warning messages indicate a problem using the "aligned" attribute without a "packed" attribute and yet it doesn't do anything with the "packed" attribute when specified. I'm using CCS version 4.2.4.00033 and the DM3730 uses an ARMv7 microprocessor.
The packed attribute is currently only supported for ARM devices that have hardware support for unaligned memory accesses. I'm not an ARM expert, but I think that basically means the Cortex devices.
I believe the warning message is issued for the fields that are subject to a packed attribute either because the attribute is applied directly to the field or because it is applied to the containing type. Thus it did not really accept the attribute in PACK_STRUCT_BEGIN.
I find it a bit odd that ignoring a packed attribute only issues a warning. Seems like this would almost always lead to bad news at runtime, so maybe an error is in order.
PS. An upgrade that will support packed for all ARM devices is under way, but I do not know when it will be released. Later this year would be my guess.
I was not able to reproduce the warning messages reported by the user using the code snippet provided. I was able to compile the struct as a packed struct and achieve an alignment of 1 for the struct. The --align_structs=4 option will override the alignment of 1 for the addr field, which is probably not what the user wants.
The user can control whether unaligned accesses can be generated by the compiler by using the --unaligned_access=[on | off] option. The default for all Cortex devices is on. My understanding is that Cortex-A8 does support unaligned accesses, but I do not know if the DM3730 has disabled that capability. If the option is set to off, I believe the compiler will reject the packed attribute.
There was a compiler bug, SDSCM00038262, where the compiler would generate unaligned loads and stores using VLDR and VSTR instructions, which do not support unaligned accesses. This was fixed in version 4.7.2 of the compiler. I recommend updating to that release or even better the 4.9.0 release since the 4.7 branch is no longer supported.
I'm currently using Code Composer Studio with compiler version 4.6.5. Before I update the compiler I would like to try a build using the --unaligned_access=on option (without the --align_structs option). How do I specify this option in the project build? I can't find a predefined compiler option in the C/C++ Build properties nor a way to add this option.
The option --unaligned_access is not supported in the v4.6.5 ARM compiler.
Thanks and regards,
-George