I was just experimenting moving a project from ccs 3.3 to 5. It is a custom board using c6713 dsps. After working out a few kinks it appears to compile fine and I can step through it on the debug perspective. I wanted to check out some of the RTA functions that I had used previous on CCS3.3. They are grayed out on the menu and I can't get them to a clickable state.