Other Parts Discussed in Thread: MSP430G2553
I would like to run the terminal in CCSv5 to communicate with msp430g2553 on LaunchPad via UART. (Hardware UART and cross jumper to switch rx,tx)
But when I run Terminals (View >> Other >> Remote Systems >> Terminals), the terminal window appears but there is no "Terminal Settings" button.
In the Terminals window is just an instruction:"To open a terminal, right-click the Terminal subsystem under the target. Then select 'Launch Terminal' from the context menu."
Version of the CCS: 5.1.0.201105121800
OS: Win 7 Pro, 32bit, SP1