This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 11.2.0 build error

Hello,

This is my first time working with CCS (Code Composer Studio). I'm using CCS 11.2.0, and I encountered an error while building the project my instructor gave me. The error message is as follows:

"xdc.tools.configuro: Error: Can't find the platform package 'ti.platforms.tms320x28'. TI platforms are no longer shipped as part of XDCtools (C:\ti\ccs1120\xdctools_3_62_01_16_core). Please ensure you are either using a pre-3.30 version of XDCtools or you have added a product that includes your platform support along the path 'C:/ti/bios_6_70_01_03/packages/ti/platforms/tms320x28/package;C:\ti\ccs1120\xdctools_3_62_01_16_core/packages'. Check that this path names a directory containing the necessary platform support and that the platform name is properly spelled."

Interestingly, when my instructor gave me another project, the build was always successful.

I've tried various solutions, but none of them have worked so far. I'm wondering if anyone has encountered a similar problem and found a solution. I would greatly appreciate any insights or ideas.

thanks you in advance

  • Hi Ousmane,

    Can you share the name of the project you are working with and which package you obtained it from. It sounds like the project you attempted to import has references to the xdctools that it is not supported natively to your version to CCS. Are there any product/tool dependencies being referenced by your project?

    Regards,

    Ozino