Other Parts Discussed in Thread: TMS320DM6437
I installed CCS v3.3 and DVSDK provided by the DM6437 EVM package. I can build the video_preview example project and I can connect to the DM6437 EVM board and load the .out into it. But the problem is I cannot successfully run the code and debug into it. When I press "run" the status is showing "running" but actually it is not running correctly. I cannot go to the main() code by clicking "go main". Any one experienced the same problem before? I tried on different PCs, the same problem. Did I miss out something? I carefully followed the "TMS320DM6437 DVDP Getting Started Guide".
I also updated the CCS v3.3 to the latest version. The problem not solved.
Additional information (Got from Help->about):
CCS verision: 3.382.13
Integrated Development 5.98.0.393 Texas Instruments
BIOS 5.31.07
Code Generation Tools v6.0.8
Board Revision: (00.00.84)
Target Silicon Revision (00.00.02)