The C6000 Compiler Tools version 7.3.0 Production Release is now available.
If you are using the Compiler Tools from within CCS, use the Software Updates tool in the CCS Help menu to obtain 7.3.0.
For users not using CCS, the compiler tools can be downloaded from the following location:
https://www-a.ti.com/downloads/sds_support/TICodegenerationTools/download.htm
Here are the highlights of this release:
This compiler has improvements to increase the performance of certain “control-code” loops.
This compiler has improvements that increase the performance of certain C6600 loops.
In addition to increases in performance for C6600 loops, other loops have improved performance. In internal testing, 3.4% of C64+ loops show improved performance. Those loops that improve show increased performance by a geomean of 130%.
This compiler supports new compiler and linker options that enable creation of object files and dynamic object modules that are compliant with the C6000 Linux ABI as set forth in the C6000 EABI Specification (SPRAB89.pdf). This release supports the capability to create C6000 Linux ABI compliant object files that can be incorporated into a dynamic executable object or a dynamic shared object (DSO). It also supports the creation of dynamic executables and dynamic shared objects (DSO) that are C6000 Linux ABI compliant. This dynamic executable or DSO can then be incorporated into a dynamic process system which utilizes dynamic modules that are created by the TI tools and/or the GCC tools. For further details on the C6000 Linux ABI, please see the C6000 EABI Specification (SPRAB89). For further details about support for the C6000 Linux ABI in the C6000 Code Generation Tools, please see the C6000 Linux Support wiki site:
http://processors.wiki.ti.com/index.php/C6000_Linux_Support
Please see the README.txt file in the v7.3.0 Compiler Tools package for additional information.