Other Parts Discussed in Thread: MSP430F5328, MSP430F5438
OK. I cracked open the cellophane off of the Wiki today and went through the S/W Install Instructions at:
http://processors.wiki.ti.com/index.php/MAVRK_Software_Installation_Guide
All went relatively smooth (yes, I didn't read through the install instructions completely, and yes, I had to re-install Putty, TortoiseGIT, and GIT a few times,) and I only have ONE question. What are the GREEN CHECK MARKS next to all of the Explorer directories? Backup verification? I don't HAVE those!
Then, I started the My First MAVRK Application tutorial.
http://processors.wiki.ti.com/index.php/Software_-_My_First_MAVRK_Application_(Using_Code_Composer)
Eventhough I have IAR tools installed (I HATE IAR's GUI,) I decided to use CCS. I uninstalled CCSv4 and installed CCSv5. This is due to some ambiguity in the MAVRK docs on whether the user NEEDS CCS v5 or not. According to the My First Application tutorial - the answer is No.
So, I am running CCS v5.1 M6 release. BTW, when CCS came up and the Welcome window tried to come up, I got a lot of Permission Denied errors - but that's a CCS issue.
I did run into one issue right out the gate with CCS v5.1. After I imported and built the project, started a debugging session, downloaded the code to my MAVRK board, and hit the GO button, when I stopped execution and tried to re-start execution, nothing happened on the board!!!
I terminated the debug session. I then tried setting a bunch of breakpoints in Template main (on EVERY LED toggle,) and walked through all of them, I then tried RUN -> Skip all breakpoints, which looked like it would work, but then I hit the GO button again and nothing happened. I terminated the debug session again, and restarted it, hit the GO button and the program executed flawlessly skipping all my breakpoints.
Someone should look into THAT issue - again, likely a CCS v5 issue.
Hey! On another note. I LOVE my MAVRK board - Thank You! I didn't know what to make of the AFE Breakout board, but now that I've run through the My First App. Tutorial - VERY COOL! WOW!! Those LEDs are getting TOO hard to see! I didn't even know they were there!!