Other Parts Discussed in Thread: CCSTUDIO, SYSCONFIG
Hello,
Minor UI problems.
(a) I have been using CCSTUDIO 12.1 and want to upgrade to CCS 12.3 but still use the compiler that comes with CCS 12.1 (v2.1.2.LTS).
Using the existing tool discovery path 'C:/ti/ccs1230' as a template, compiler discovery does not work for the equivalent path 'C:/ti/ccs1210':

Eventually I found that explicitly adding the compiler path will add the old compiler:

It's not much of a discovery if I have to specify the path explicitly.
(b) After manual installation of the bundled SysConfig 1.14.0 from CCS12.1, the path shown is the path to the standalone version:

(c) Cannot remove incorrectly installed standalone SysConfig 1.14.0. Uninstall button greyed out.