Other Parts Discussed in Thread: TMS320DM6437
Hi,
A customer installed CCS v3.3 and DVSDK provided by the DM6437 EVM package. He can build the video_preview example project and can connect to the DM6437 EVM board and load the .out into it. But the problem is he cannot successfully run the code and debug it.
When he presses "run" the status is showing as "running" but actually it is not running correctly. He cannot go to the main() code by clicking "go main". He tried this on different PCs, but faced the same problem. He has followed the "TMS320DM6437 DVDP Getting Started Guide". He also updated the CCS v3.3 to the latest version. The problem is still not solved.
Additional information (Got from Help->about): CCS version: 3.382.13
Integrated Development 5.98.0.393
Texas Instruments BIOS 5.31.07
Code Generation Tools v6.0.8
Board Revision: (00.00.00)
Target Silicon Revision (00.00.00)
Regards,
Prachi
82406126