This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to change the default location for the workspace in CCS Theia?

How can I change the default location for the workspace in CCS Theia?

  • A different folder can be specified for the workspace. To do this, go to: File → Open Folder... and specify the folder to switch to.

  • By default, and when running on Win 10, CCS Theia creates a workspace under ...users/UserName/workspace_ccstheia. When a different folder is created, it then becomes the default folder until you select a different folder.

    There is no specific setting in CCS Theia where you change the default workspace folder. You either select an existing one or create a new one through the Open Folder command. Therefore, the currently selected workspace remains the default workspace until you select another one or create a new one.